Error Statistics

Associated with: OPC XML-DA scanners

The Error Statistics attribute shows the number of errors generated during any of the read or write operations that are summarized by the Comms Statistics attribute.

The Error Statistics indicate the number of occurrences of each of the following since the scanner was last restarted:


Disclaimer

ClearSCADA 2017 R3