Configuring Pager Devices in ClearSCADA

For ClearSCADA to make use of the pager/mobile telephone messaging features, you need to configure:

Before you can configure these items, you need to have access to, or an understanding of, the settings of the pagers and mobile telephones that are going to be used with your system. This is because many of the settings you need to define in the ClearSCADA database have to correspond to the settings of the relevant pager equipment. For example, when you configure a User account, you will need to enter a Pager ID that corresponds to the pager number or mobile telephone number of the device owned by the user of the account.

You also need to know which of the optional features are required for your pager items. The optional features include alarm views, alarm redirections, and User methods.

When you have the pager settings information and you understand which optional features are required, you can proceed with configuring the pager items on your system:

  1. Install the Pager Driver on each of the ClearSCADA servers in your system and check that it is running. To install the Pager Driver, simply re-install ClearSCADA and set the installation to include the Pager Driver.
  2. Check that appropriate Pager settings are in place on the ClearSCADA server (see Configuring Pager Server Settings).
  3. Configure a Pager Service for each protocol that is required (see Configuring a Pager Service). You will need to configure additional Pager Services for each variation in the protocol settings, for example, if you need SMS Pager Services with different timeout settings, you will need an SMS Pager Service item for each variation.
  4. Configure a Pager Channel to represent each connection between the Pager Driver and the Service Provider (see Configuring a Pager Channel).
  5. Configure the User accounts for those members of staff that are going to need to receive messages on their pager devices or mobile telephones. Each of these User accounts has to:
  6. For more information on defining the Pager ID and the Pager Service, see Configuring a User Account's Pager Properties.

When you have configured the properties described above, you can send messages manually to those system users that have a pager device/mobile telephone. For further information, see Sending a Message Manually.

If automatic messaging is required, some further configuration is needed:

When you have successfully configured the pager items, they will be available for use in the ClearSCADA database. You can use the pager items with the core ClearSCADA features, including Lists, Actions and Mimics. For example, it is possible for operators to filter the Alarms and Events Lists so that they only display those entries that are associated with the state of Pager Comms. For further information:


Disclaimer

ClearSCADA 2017 R3