SCADAPack Modbus Controller Status Attributes

In addition to the Advanced Modbus Controller Status Attributes, SCADAPack Modbus controllers support SCADAPack-specific status attributes. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

NOTE: This section is about status attributes that are specific to this driver. In addition to the status attributes mentioned here, this driver's extension drivers might support further status attributes. For information about driver-specific status attributes that are not covered in this section, see the relevant extension driver guide.


Disclaimer

ClearSCADA 2017 R3