Configure the Basic Flow Run Properties

Use the fields at the top of the Flow Run tab on the Flow Run Form to specify these properties:

Further Information

For more information, see Requesting Confirmation of Action Requests in the ClearSCADA Guide to Core Configuration.


Disclaimer

ClearSCADA 2017 R3