Liquid Flow Run Properties

For a Liquid Flow Run use the fields on the Liquid tab of the Flow Run Form to Configure the Flow Run Properties.

You can configure these properties directly in ClearSCADA, or read the configuration into the ClearSCADA database (see Configure or Read the Flow Run Configuration).

With the properties listed below, you can either Configure or Read the Flow Run Configuration.


Disclaimer

ClearSCADA 2017 R3