SCADAPack x70

Remove Logic Application

Associated with: SCADAPack x70 Device Configuration items

Security permission required to access this pick action: Control

Use the Remove Logic Application pick action to remove the local copy of the SCADAPack x70 logic application that has been imported into ClearSCADA from the SCADAPack RemoteConnect configuration software (see Import from RemoteConnect).

The Remove Logic Application pick action is only available in ClearSCADA if a logic application has already been imported into ClearSCADA from RemoteConnect - you use the Import from RemoteConnect pick action to do this.

When you use the Remove Logic Application pick action, a confirmation dialog box is displayed (see Action Requests that Require Confirmation). The confirmation dialog box is displayed regardless of the settings used to determine whether similar confirmation dialog boxes are displayed for other types of pick actions.

If using this pick action with the Automation Interface, you need to specify the method name RemoveRTZ.


Disclaimer

ClearSCADA 2017 R3