Add and Configure an SQL Export

In order to export the result of an SQL Query and define the location and format in which that result is to be exported, you need to configure at least one SQL Export item in the ClearSCADA database. You need to configure a separate SQL Export item per SQL Query.

To add an SQL Export item to your database:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right click on the Group or Group Template within which you want to add an SQL Export.
    A context sensitive menu is displayed.
  3. Select the Create New option.
    A further menu is displayed.
  4. Select the Other option.
    A further menu is displayed.
  5. Select SQL Export option.
    An SQL Export item is added to the database. The entry is highlighted, ready for you to define its name.

Configure each SQL Export item using the SQL Export Form. For general information on working with Forms, see Working with Forms.

The SQL Export Form has several tabs:

Use the Export SQL Query Result pick action to export the result of an SQL Export item’s SQL Query, using the settings specified on the configuration Form.


Disclaimer

ClearSCADA 2017 R3