Clients (WebX)
            The WebX branch of the Server Status Tool includes a Clients category. The Clients categoryprovides status information about each WebX client that is connected to the server.
                
            
The status information for each WebX client is categorized under these headings:
- Address—The IP address of each client.
 - Links—The number of links between the WebX client and the server.
 - Up Time—The amount of time since the WebX client connected to the server.
 - Licensed—Indicates whether the client has a valid license (Yes or No).
 
The number of clients varies according to the size of your system.
The Clients (WebX) category is often used to check that WebX clients have valid licenses (they will be unable to connect to the server if they have invalid licenses) and also to determine which WebX clients have a connection to the server.
Further Information