WebX Status Information
            The Server Status Tool provides status information that is organized into groups of categories, each of which contains sub-categories. The WebX group provides status information about any WebX clients that are connected to the server and the cookies, links and threads that they use. The WebX group contains the following sub-categories:
                
            
- Clients (WebX)—provides status information about each WebX client that is connected to the server
 - Cookies—provides status information about each WebX cookie that is currently in use
 - Links (WebX)—provides status information for the connections between the server and any WebX clients
 - Threads—provides status information about the threads that are used to service the WebX links (links between the server and the WebX clients).
 
Further Information
WebX: see WebX Client
Is WebX activity causing a high load on the server? see WebX Client Activity.