Configuring Digital Points

The Simatic S7 driver supports 1-, 2-, and 3-bit Digital points.

Digital points can be physical points that exist on Simatic S7 PLCs, or calculated states that reside within Simatic S7 registers.

Configure the properties for each Digital Point using the fields on the Simatic S7 Digital Point Form.

This section covers configuration of properties on the Simatic S7 tab of the Form (see Configure the Simatic S7 Point Properties).

For information on the fields on the Digital Point tab, see Defining Digital Point Details in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on the Control tab, see Define the Control Settings for a Digital Output Point in the ClearSCADA Guide to Core Point Configuration.

For information on the Control Checks tab, see Configuring Control Checks Settings in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R3