Configuring Analog Points

ClearSCADA can retrieve various forms of diagnostic data from a Trio radio. For each item of diagnostics data that can be in one of a range of numeric values, you need to configure a Simple Trio Diagnostics Analog Point in the ClearSCADA Database.

Configure the point’s properties using the fields on the Simple Trio Diagnostics Analog Point Form. The Form has several tabs.

Use the Trio Diagnostics tab to:

The Analog Point tab contains properties that are common to analog points on many drivers (see Defining Analog Point Details in the ClearSCADA Guide to Core Point Configuration).

The fields on other tabs are common to points on many drivers (see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers).


Disclaimer

ClearSCADA 2017 R3