Welcome to the WebX System Configuration Guide

Welcome to the ClearSCADA Guide to WebX System Configuration. This guide is designed to help you understand how the ClearSCADA WebX Server is configured to connect to your ClearSCADA system, and how to edit or add further connections if required.

The WebX System Configuration applet to which this guide refers is available on machines on which the WebX server is installed.

Intended Audience

The ClearSCADA Guide to WebX System Configuration is aimed at administrator level users who are responsible for the initial set-up of WebX System connections and settings. For information about WebX features, you should refer to the ClearSCADA Guide to ViewX and WebX Clients.


Disclaimer

ClearSCADA 2017 R3