MessageOff

Description

The Off message for the tag. This property applies to discrete tags. The Off message is the message associated with the FALSE state of the discrete tag. The maximum number of characters is 64. A discrete tag set to 0 is in the FALSE state. All tags created by ClearSCADA are analog tags (including digital points), and therefore this property is not applicable.

ClearSCADA Metadata Field

WH_MessageOff

Default Value

The default value for this property is an empty string.

Type

String.

Further Information

MessageOn


Disclaimer

ClearSCADA 2017 R3