MessageOn

Description

The On message for the tag. This property applies to discrete tags. The On message is the message associated with the TRUE state of the discrete tag. The maximum number of characters is 64. A discrete tag set to 1 is in the TRUE state. All tags created by ClearSCADA are analog tags (including digital points), and therefore this property is not applicable.

ClearSCADA Metadata Field

WH_MessageOn

Default Value

The default value for this property is an empty string.

Type

String.

Further Information

MessageOff


Disclaimer

ClearSCADA 2017 R3