Configure the X-Axis Label

You can specify a label for the axis. The label is a text string that identifies the axis. You specify the label using fields in the X-Axis Properties window (see Configure the X-Axis Properties).

Use the Label section of the window to specify the properties associated with the axis label:

The axis label's position is fixed at 'Center' if the range labels are shown (in which case, the Position combo box is 'grayed out' and unavailable for use). For information about range labels, see Configure the Axis Range.


Disclaimer

ClearSCADA 2017 R3