Supported Features and Functionality

This topic summarizes some of the features and functionality for which the Advanced Trio Diagnostics driver provides support (when applicable to the type and model of radio and the communications setup). Select the relevant heading to display information about a particular feature or function. Use this topic in conjunction with Trio Radio Series Supported by the Advanced Trio Diagnostics Driver to determine the features and functions that each series of radio supports. For information not included here or elsewhere in this guide, see the documentation supplied with your Trio radio equipment.


Disclaimer

Geo SCADA Expert 2019