Adjust the Columns on an Alarms List or the Alarm Banner

Alarms Lists and the Alarm Banner display these columns by default:

Order and Names of Columns Width of Alarm Banner Column on a ViewX Client Width of Alarms List Column on a ViewX Client Width of Alarms List Column on a Virtual ViewX Client
Severity

82

80

75

Time

282

160

150

Source

301

312

350

Message

444

275

450

Category

200

183

100

System

200

200

---

Area of Interest

200

198

200

Suppressed Alarm Count

200

200

200

The Area of Interest column is only displayed if the Area of Interest feature is enabled on your system (see Restrict Alarm and Event Access to Specific Areas of Interest).

If you are working with multiple databases within a ViewX client you should ensure that the Area of Interest feature is configured the same way for all systems.

The System column is only displayed on a ViewX client that is configured to access Multiple Databases.

You can use the Alarm Columns window to adjust the columns that are displayed on an Alarms List or the Alarm Banner (see Use the Alarm Columns Window to Change the Alarms List or Alarm Banner Columns). You can use the window to:

If the Allow Column Resizing check box is selected on the Alarms and Events tab of the Options window (see Specify the Preferred Alarm Banner and Alarms List Options on a ViewX Client), you can also:

Users with the required permission can add additional columns to the Alarms Lists and Alarm Banner, if required (see Configure Additional Alarm Columns).


Disclaimer

Geo SCADA Expert 2019