Filter Wildcards

When filtering an Alarms List or Alarm Banner by Source, you can include wildcard characters in the filter criteria. Wildcard characters allow a single character to match any of one or more unspecified characters. The Sources filter on the Alarms List or Alarm Banner’s Filter window supports these wildcard characters:

Further Information

Pre-filter alarms by Alarm Source using the Alarm Filter String: see Specify a Default Alarm Filter.

(The filter wildcards that are supported by Lists other than the Alarms List differ to the above—for information, see Filter Wildcards in the Geo SCADA Expert Guide to Lists.)


Disclaimer

Geo SCADA Expert 2019