Specify whether the Position of the Highlighted Alarm Changes when New Alarms are Raised

If one or more alarms are selected in the Alarms List or Alarm Banner, a new alarm will cause:

Or:


The behavior that applies to your ViewX client is dependent on the Maintain Position of Highlighted Alarm when New Alarms Arrive setting. This setting is shown on the Options window’s Alarms and Events tab.

By default, the Maintain Position of Highlighted Alarm when New Alarms Arrive setting is selected, which means the focus will remain on the selected alarms. But if required, you can clear the setting so that the Alarms List or Alarm Banner will always focus on a new alarm.

To change the setting:

  1. Log on via a user account that has the Configure Options permission, and then display theOptions window.
  2. Select the Alarms and Events tab.
  3. Select or clear the Maintain Position of Highlighted Alarm when New Alarms Arrive as required.
  4. Select the OK button to confirm your selection.

The above setting applies to highlighted alarms that are displayed in Alarms Lists and the Alarm Banner on the local ViewX client. You use a different setting to define whether the position of highlighted alarms is maintained in Alarms Lists that are displayed on Virtual ViewX clients (see Define the Alarms List Order and Background Settings in the Geo SCADA Expert Guide to Server Administration).


Disclaimer

Geo SCADA Expert 2019