Failed Original WebX Client or XML Client - System Connections

ATTENTION: This section and associated topics apply to the Original WebX client only.

If you attempt to access your system from an Original WebX or XML client and it is unable to establish a connection, the web browser application that you are using will display a ‘connection failed’ message.

Original WebX and XML clients use the built-in Web Server to connect to the Geo SCADA Expert server. The settings for the Web server are configured using the Server Configuration Tool, see Web Server Settings.

If your web browser displays a connection failed message, it may be because:


Disclaimer

Geo SCADA Expert 2019