Display a Form

To display a Form for a database item, perform one of the following:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Double-click on the item in the Database Bar (if you are logged on as a user that has the Double Click Edits Documents feature enabled).
    The associated Form is displayed.

or:

  1. Right-click on the item in the Database Bar.
    A context-sensitive menu is displayed.
  2. Select the Edit Properties option.
    The associated Form is displayed.

or:

  1. Right-click on the item in a Queries List.
    A context-sensitive menu is displayed.
  2. Select the Properties option.
    The associated Form is displayed.

or:

  1. Select an animated representation of the item on a Mimic. (Provided that the animated representation is associated with the item’s Object menu and provides access to the relevant menu option.)
  2. Select the Properties option.
    The associated Form is displayed.

When one database item references another database item, you can display the Form of the referenced item by:

or:

  1. Use the Display References pick action to display the list of references for the item (see Displaying a Database Item’s References).
  2. Expand the entries in the Display References window as required.
  3. Right-click on the referenced item for which you want to display the Form.
    A context-sensitive menu is displayed.
  4. Select the Edit Properties option.
    The item's Form is displayed.

Each Form has a series tabs that contain fields for particular aspects of the configuration (see Fields on Forms). Any messages relating to incomplete, incorrect, or conflicting configuration are displayed in a message area directly below the Form (see Mandatory Configuration and Invalid Configuration Messages).

Use the information within the core configuration guides and the appropriate driver-specific guide to help you configure the items in your database.


Disclaimer

Geo SCADA Expert 2019