Display the Schedule Form

To configure a Schedule, you need to display its Form. The Form contains the fields required to configure a Schedule.

To display the Schedule Form:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Right-click on the Schedule in the Database Bar.
    A context sensitive menu is displayed.
  3. Select the Edit Properties option.
    The Schedule Form is displayed.

You can use the Schedule Form to:

  1. Configure the Identification details (see Defining Identification Details).
  2. Configure any custom pick actions that are to be associated with the Schedule (see Using the User Methods Tab to Define Custom Actions).
  3. Define the type of Schedule, the time zone in which it operates and whether the schedule is in service (see Define the Basic Schedule Properties).
  4. Define when a Simple Schedule Executes.
  5. Optionally Associate a Calendar with a Daily or Weekly Schedule.
  6. Save the configuration.

Disclaimer

Geo SCADA Expert 2019