The Effects of Alarm Suppression in Geo SCADA Expert

This section explains the effect that alarm suppression has on Geo SCADA Expert.

In the bullet list below, parent alarm refers to an alarm that meets the Parent Alarm Condition criteria and is raised on the item that is configured as a Parent Alarm Object. Child alarm refers to an alarm that is raised on a database item on which the above Parent Alarm Object is specified. For more information, see Configure any Alarm Suppression Requirements.

When alarm suppression is configured:

The parent-child alarm relationship can be cascaded, so that a top level parent alarm will disable the alarms of its child items, and of the children of those child items, and so on.

For an example that demonstrates the effects of alarm suppression in Geo SCADA Expert, see Example Configuration.


Disclaimer

Geo SCADA Expert 2019