Using OPC Time Formats

Use OPC time formats for entering dates and times in Geo SCADA Expert. The formats are based on the standards that are defined by the OPC Foundation. The formats that you need to use vary, depending on the type of time or date. Within Geo SCADA Expert you can enter and display these types of dates and times:

The relevant sections in the Geo SCADA Expert documentation indicate which format you should be using to specify a time or date.

Further Information

OPC Foundation Standards: See www.opcfoundation.org

Time Zone Support in Geo SCADA Expert.


Disclaimer

Geo SCADA Expert 2019