DNP3

Upload File

Associated with: DNP3 master outstations

Security permission required to access this pick action: Retrieve Data

Use the Upload File pick action to upload any file from a Slave outstation to its master. You can use the pick action whenever the master is in communication with the Slave.

Select the Upload File pick action to display the Upload File window. The content of the window varies, depending on the File Transfer Variation supported by the outstation (see Specify Which File Transfer Routines an Outstation Supports).

Where an outstation supports the Revised g70 Variations of File Transfer routines, the Upload File window includes these fields:

Where an outstation supports the Legacy g70v1 File Transfer variation, the Upload File window includes a single Filename field. Use the field to enter the name of the file that you want to upload, and then select the OK button to perform the upload.

The location to which the file is uploaded is specified as part of the Geo SCADA Expert Server Configuration (see Define the DNP3 Master File Transfer Parameters). The file will be uploaded to that location on whichever Geo SCADA Expert server is currently the main server.

The DNP3 outstation may impose file name restrictions on the files that it holds. See the outstation documentation regarding such restrictions.

Example:

The directory on the main server into which files are uploaded from DNP3 outstations is set to C:\ClearSCADADB.

An operator selects the Upload File pick action on a particular DNP3 outstation, and specifies the file name thisfile.txt.

On execution of the pick action, Geo SCADA Expert uploads the file thisfile.txt from the DNP3 outstation, to the server location C:\ClearSCADADB.


Disclaimer

Geo SCADA Expert 2019