DNP3

Specify Which File Transfer Routines an Outstation Supports

Geo SCADA Expert is able to transfer files such as ISaGRAF applications to an outstation that supported File Transfers.

Use the fields within the File Transfer section of the DNP3 tab to specify whether an outstation supports File Transfer routines and if so, the variation that it supports.

Variation

Use the combo box to specify the File Transfer routine that the outstation supports. Choose from:

With an outstation that supports file transfers, you can use:

For more information, see Using DNP3 Specific Actions.

Requires Authentication

Applicable if the outstation supports Revised g70 Variations. Select this check box if a user name and password are required to access the outstation’s file system.

Clear the check box if user name and password authentication is not needed to access the outstation’s file system.

User Name

Only applies if the outstation supports Revised g70 Variations that require authentication. Specify a user name that provides read/write access to the outstation’s file system, to enable Geo SCADA Expert to transfer files to and from the outstation.

Password

Specify the password that, combined with the User Name above, provides read/write access to the outstation’s file system.

Event Polling Interval

Use to specify the frequency at which Geo SCADA Expert is to poll the outstation for file events during asynchronous file transfers. Enter the required interval in the OPC Time Format.


Disclaimer

Geo SCADA Expert 2019