Configure General Properties

Use the fields at the top of the Binary Point tab to define the general properties of a DNP3 SCADAPack binary point. For further information on most of these properties, see Configure Common Properties of DNP3 SCADAPack Points in this guide, and see Configure General Properties in the Geo SCADA Expert Guide to the DNP3 Driver. Properties that are specific to DNP3 SCADAPack Binary points are explained below:


Disclaimer

Geo SCADA Expert 2019