Add a New Driver to an Existing Geo SCADA Expert System

This section is for system administrators that are installing a new driver on a system on which other drivers are already installed.

When adding a new driver to an existing Geo SCADA Expert system, you need to:

  1. Ensure that your system has a valid license for the new driver. (Use the License Details window to check whether a valid driver license existssee Server License Settings - Geo SCADA Expert.)
  2. Use the Geo SCADA Expert Installation Wizard to select the driver component(s) that you need to install (see Install a Driver in Geo SCADA Expert).

    Remember that if you are installing an Extension Driver, you also need to ensure that its ‘parent’ driver is installed and suitably licensed.

  3. Configure any driver-specific server settings for the new driver. (Not all drivers have server settings that are driver-specific—the relevant driver guide will summarize any settings that do exist.)
  4. Add the various driver-specific items—channels, points, and so on—to your system and configure those items in the database (see the relevant driver guide and, if applicable, see Configure a Channel’s Connection Properties).

    Remember that by default, Geo SCADA Expert does not store point data historically—if you want Geo SCADA Expert to store data historically for a particular point, you need to enable Historic on the configuration Form for that point, see Defining Historic Details for a Point.

  5. If required, specify the alarm conditions for which any new point types are to have Multiple Point State Alarms. (For information on this feature, see Multiple Point State Alarms. For information on setting up multiple point state alarms, see Point State Alarms)
  6. Set up the required security for the newly added driver items (see the Security Guide).

    (Remember that security permissions are assigned on a per item/per group basis, whereas access to the various features and functions is assigned on a per user/per user group basis.)

Further Information

Set up the Drivers on a New Geo SCADA Expert System.


Disclaimer

Geo SCADA Expert 2019