Cancel Promoted Dial Out

Associated with: Outstation sets; PSTN outstations or outstations with PSTN fallback; Slave PSTN outstations

Security permission required to access this pick action: Promote

This pick action is only available if the rate at which Geo SCADA Expert is dialing out to an outstation is currently promoted (see Promote Dial Out).

Use the pick action to terminate the current promotion. Once executed, Geo SCADA Expert reverts to dialing the outstation at its usual rate.


Disclaimer

Geo SCADA Expert 2019