Promote Dial Out

Associated with: Outstation sets; PSTN outstations or outstations with PSTN fallback; Slave PSTN outstations

This pick action is only available for an outstation or set on which:

Use the Promote Dial Out pick action to temporarily increase the rate at which Geo SCADA Expert retrieves data from one or more outstations (see Temporarily Increasing the Frequency with which an Outstation is Called in the Geo SCADA Expert Guide to Advanced Drivers). When this pick action is used on an outstation, Geo SCADA Expert sends One Shot requests to that particular outstation at a promoted rate, for the duration of the promotion. When executed on a set, Geo SCADA Expert sends One Shot requests at a promoted rate to each of the outstations on that set. For more information on the order in which Geo SCADA Expert contacts the outstations in a set, see One Shot.

Select the pick action to display the Promote Dial Out window.

Use the fields and check box to specify the required promotion:

The Promoted Dial Out defaults for the outstations on your system are specified using the Geo SCADA Expert Server Configuration Tool (see Define the Default Promoted Dial Out Settings in the Geo SCADA Expert Guide to Server Administration.

The Dial Out Promoted status attribute indicates whether dial-outs are promoted on a set or outstation.

Also see Cancel Promoted Dial Out.


Disclaimer

Geo SCADA Expert 2019