Override

Associated with: Points on which the Override feature is supported and enabled

Use the Override pick action to temporarily override a point’s value. You might want to use this action, for example, to specify a suitable value if Geo SCADA Expert has detected a known fault that is causing an incorrect value to be reported. Once the detected fault has been corrected, use the Release Override action to revert back to using the point’s actual value—the value that is being reported by the outstation or scanner.

The Override pick action is only available on a point on which:

Most drivers support master station overrides, whereby you override the value at the server. Some drivers support outstation overrides—with such drivers, the driver-specific documentation explains any differences in functionality to that covered in this section.

Select the Override pick action to display the Override window.

Specify the required override value in the Value field. Depending on the type of point, you may be offered a combo list of point values, or need to specify a value within a particular range. The range or values from which you can choose are determined by the point’s configuration.

Whenever a point is overridden:


Disclaimer

Geo SCADA Expert 2019