Points Used on EcoStruxure Web Services Scanners

EcoStruxure Web Services Scanners read and write to data on EWS servers. You need to map the data on each EWS server to suitable EcoStruxure Web Services Points within the Geo SCADA Expert database, to enable Geo SCADA Expert to handle the data in a similar way to other point data on the system (for instance, in order to monitor state changes, raise alarms, or execute controls).

The Simple EcoStruxure Web Services Client Driver can support any of the point types that are listed below. You need to configure those point types that present the EcoStruxure Web Services node data in a suitable format within the Geo SCADA Expert database.

For information on creating a point and displaying a Point Form, see Configuring a Point in the Geo SCADA Expert Guide to Core Point Configuration.

For information on configuring fields on the EcoStruxure Web Services tab, see the rest of this section, which explains how to:

For information on configuring fields on the <Point Type> tab, see the references below:

For each point, use the Enabled check box on the Control tab to specify whether a particular point is used as an Input point to retrieve data, or as an Output point to write data to an EWS server. For information on the Control tab, see the Geo SCADA Expert Guide to Core Point Configuration.

For fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.


Disclaimer

Geo SCADA Expert 2019