Configuring Analog Points

The Kingfisher driver supports Analog Input points and Analog Output points.

With the Kingfisher protocol, the preferred setup is for analog inputs to report state changes back to a Master outstation from a Remote outstation. With such a setup, use the standard Kingfisher Remote Outstation Change of State programming to report any state changes to the Master outstation.

Configure the properties of each analog point using the fields on the Kingfisher Analog Input Point Form, or the Kingfisher Analog Output Point Form, as appropriate.

This section covers configuration of properties on the Analog Point tab of both Kingfisher Analog Point Forms, and the properties on the Control tab of the Kingfisher Analog Output Point Form.

 

Use the Analog Point tab to:

 

For Kingfisher Analog Output points, there are two additional tabs: a Control Tab and a Control Checks tab.

Use the Control tab to:

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers.


Disclaimer

Geo SCADA Expert 2019