Define the Permitted Scan Durations

Use the second Scan Parameters section on a Kingfisher Direct Channel Form’s Scan Parameters tab to define the permitted scan durations for the direct channel.

The Geo SCADA Expert server uses the scan times to determine whether the outstations that communicate via the selected channel are scanned within a suitable time. If not, the server generates alarms relating to the scan status.

Before you attempt to define the scan durations, you need to have an appreciation of the scanning procedure, and the different types of scans (see Scanning Direct Outstations on the Kingfisher Driver).

Use these fields to specify the Quality Factor and permitted scan durations for a channel. You can enter the durations directly in each scan field, or use the Interval Window (accessed via each field’s browse button) to specify the required durations.


Disclaimer

Geo SCADA Expert 2019