The Logic Tab

The Logic tab appears on the ViewX ribbon when the active window in the Document Display Area comprises a Logic Program.

The Logic tab contains the following command groups:

Build

The Build group includes commands that you use when you compile one of the following Logic programs:

Debug / Breakpoints

The Debug and Breakpoints groups include commands that you use to:

Library

The Library group includes the Libraries command, which you use to reference an ST Library or Function Block Library (see ST and Function Block Libraries).

View

The View group includes the following commands:

Variables

Display Settings

Update Interval

Allows you to change how often your Geo SCADA Expert client PC requests updates for a Logic Program. See the following topics:

Connection Values

Displays the current value for the connections on a Ladder Diagram and Function Block Diagram (see Viewing the Values on a Function Block Diagram and Viewing the Values on a Ladder Diagram).


Disclaimer

Geo SCADA Expert 2019