Create Another Analog Point

Add another MQTT JSON Schema A Analog Point to the database. Geo SCADA Expert will use this point to store the data that it retrieves and processes from the other analog tag for which the MQTT client publishes data.

When you create the point, you can leave most of the configuration fields at their default values.

On the Analog Point tab of the configuration Form, the only fields that you need to change for this tutorial are:

On the Historic tab:

Save the configuration.

Once you have configured the analog point, you can proceed to Create a Mimic on which to Display the Points.


Disclaimer

Geo SCADA Expert 2019