Configuring an NTP Monitor Scanner

An NTP Monitor Scanner is logical functionality that runs within Geo SCADA Expert and scans for NTP data on an NTP Server. An NTP server might be the ‘reference’ clock itself, or a machine that synchronizes its own clock with the ‘reference’ clock (see Understanding NTP Stratum Ranking and how this Affects Clock Accuracy).

Configure the NTP Monitor Scanner properties using the fields on the NTP Monitor Scanner Form.

The Form has several tabs. This section covers fields on the Scanner tab that are specific to the NTP Monitor driver (see Configure the Scanner Properties).

For fields on the other tabs, see Tabs That are Common to Many Configuration Forms in the Geo SCADA Expert Guide to Simple Drivers.


Disclaimer

Geo SCADA Expert 2019