Configuring Analog Points

In addition to the analog points mentioned below, Geo SCADA Expert can support other types of analog point using a SCADAPack Modbus Extension Driver. For information on any SCADAPack Modbus points not listed below, see the relevant SCADAPack Modbus driver extension guide.

The SCADAPack Modbus driver supports SCADAPack Modbus Analog Input points and Analog Output points.

Configure the properties for each analog point using the fields on the SCADAPack Modbus Analog Input Point Form, or the SCADAPack Modbus Analog Output Point Form, as appropriate.

This section covers configuration of properties on the Analog Point tab of each Form, and the properties on the Control tab of the SCADAPack Modbus Analog Output Point Form. Some of these properties are identical to the properties that are supported by analog points on the driver's 'parent' Advanced Modbus driver. For information about such properties, follow the links below to access the relevant sections in the Geo SCADA Expert Guide to the Advanced Modbus Driver.

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers.

For SCADAPack Modbus Analog Input or Analog Output points, use the Analog Point tab to:

For SCADAPack Modbus Analog Output points there are two additional tabs: a Control Tab and a Control Checks tab.

Use the Control tab to:

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).


Disclaimer

Geo SCADA Expert 2019