Configuring Digital Points

The SCADAPack Modbus driver supports 1-, 2-, and 3-bit Digital Input points and Digital Output points.

Configure the properties for each Digital point using the fields on the SCADAPack Modbus Digital Input Point Form, or the SCADAPack Modbus Digital Output Point Form, as appropriate.

This section covers configuration of properties on the Digital Point tab of both SCADAPack Modbus Digital Point Forms, and the properties on the Control tab for Digital Output points. The properties on other tabs are common to points on many advance drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).

Use the Digital Point tab to:

For SCADAPack Modbus Digital Output Points there are two additional tabs: a Control Tab and a Control Checks tab.

Use the Control tab to:

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).


Disclaimer

Geo SCADA Expert 2019