SCADAPack x70

Configure Modbus Point Scanner Settings

The Modbus Point Scanner section of the Modbus tab allows you to configure how the SCADAPack x70 reads and writes with points associated with the Modbus Slave device.

Operation

Use this combo box to specify whether the SCADAPack x70 reads from, or writes to, the point on the Modbus Slave device. Select from Read, Write, or Read/Write.

Ensure that the Operation is set to Read if the Modbus Point Scanner is to read counter data. (As the driver does not write to counters.)

If writing to analog data, be aware that the option specified for the associated Modbus Slave Device's Write Holding Registers setting might impact on the availability of some Modbus Data Type options. The options define the type of analog data to which the Scanner can write (see Configure Modbus Point Scanner Configuration).

Write Outputs

This combo box will only be available if you set the Operation to Write. Use this combo box to specify when the SCADAPack x70 writes to the point on the Modbus Slave device. Select from the following:

At Scan Rate

Write to the point at the Default Scan Rate configured for Slave device, see Configuring a Modbus Slave Device or at the Scan Rate defined on this form (see Scan Rate below).

On Change

Write to the point when the point value changes.

At Scan Rate and On Change

Write to the point at both the Default Scan Rate configured for the slave device, and when the point value changes (see Configuring a DNP3 SCADAPack E Modbus Slave Device ).

Operation for Offline Devices

This combo box will only be available if you set the Operation to Read/Write. Use this combo box to specify the operation the SCADAPack x70 should perform while the point is offline.

Unsuccessful Write Operation

This combo box will only be available if you set the Operation to Read/Write. Use this combo box to specify the operation that should occur when a write failure occurs. Either Revert to the previous operation or Retain the current operation.


Disclaimer

Geo SCADA Expert 2019