SCADAPack x70

Configure Modbus Point Scanner Configuration

The Configuration section allows you to configure the general point scanning properties.

Modbus Data Type

Use this combo box to specify the format of the point value. The options that are available vary, depending on the Object Type (see below). The options comprise a combination of the following:

Discrete

The value is formatted as a discrete number (digital points only).

INT

The value is formatted as signed 16-bit data. Each INT comprises 1 Modbus register.

UINT

The value is formatted as unsigned 16-bit data. Each UNIT comprises 1 Modbus register.

DINT

The value is formatted as signed 32-bit data. Each DINT comprises 2 Modbus registers (analog points only).

When the Scanner's Operation is set to 'Write' or 'Read/Write', this option is only available if the associated Modbus Slave Device's Write Holding Registers property is set to 'Multiple (Function Code 16)'. For information about configuring the latter property, see Configure Modbus Slave Device Configuration Settings. For information about configuring the Modbus Slave Scanner's Operation property, see Configure Modbus Point Scanner Settings.

UDINT

The value is formatted as unsigned 32-bit data. Each UDINT comprises 2 Modbus registers (counter points only).

Real

The value is formatted as an IEEE 32-bit single-precision floating point value. Each REAL comprises 2 Modbus registers (analog points only).

When the Scanner's Operation is set to 'Write' or 'Read/Write', this option is only available if the associated Modbus Slave Device's Write Holding Registers property is set to 'Multiple (Function Code 16)'. For information about configuring the latter property, see Configure Modbus Slave Device Configuration Settings. For information about configuring the Modbus Slave Scanner's Operation property, see Configure Modbus Point Scanner Settings.

Modbus Register Start Address

Enter the first address in the Modbus register range that you want scanned.

The valid range depends on the Modbus data type:

Discrete

1 to 9999 or 10001 to 19999

INT, UINT, DINT, UDINT and Real

30001 to 39999 or 40001 to 49999

Modbus Register Quantity

Enter the total number of Modbus registers that you want to be scanned and mapped.

This parameter is only configurable after a valid Modbus Register Start Address is entered. It is automatically updated based on the Modbus Data Type. For example, DINT and REAL data types require twice as many Modbus Registers as UINT or INT data types.

Object Type

Use this combo box to specify the type of SCADAPack x70 Configuration item to which the Modbus registers are to be mapped.

Choose from:

Analog

The Modbus Point Scanner is being used to read, or write to, analog data.

Use the Mapping tab on the relevant SCADAPack x70 Analog Configuration item(s) to reference this Modbus Point Scanner and specify the Modbus Register addresses at which each analog is located.

Digital

The Modbus Point Scanner is being used to read, to write to, digital data.

Use the Mapping tab on the relevant SCADAPack x70 Digital Configuration item(s) to reference this Modbus Point Scanner and specify the Modbus Register addresses at which each digital is located.

Counter

The Modbus Point Scanner is being used to read counter data. This option is only available when the Modbus Point Scanner's Operation is set to 'Read'. (You specify the Operation in the Modbus Point Scanners section of the tab.)

Use the Mapping tab on the relevant SCADAPack x70 Counter Configuration item(s) to reference this Modbus Point Scanner and specify the Modbus Register addresses at which each counter is located.

Scan Rate

Enter the frequency rate at which the SCADAPack x70 scans the point. Enter the rate directly in the field (see Specify a Time Period in the OPC Time Format) or use the Interval Window to specify the rate that you require, (see Configure Modbus Slave Device Configuration Settings).

To use the same scan rate as the Modbus Slave, leave the default setting of 0.

Timeout

Use this check box to set the amount of time that the SCADAPack x70 should wait for a response when it scans the point on the Modbus Slave device. To use the same timeout as the Modbus Slave, leave the default setting of 0.

If the SCADAPack x70 does not get a response in this time, it will try the scan again until it exceeds the Maximum Consecutive Timeouts count. If the SCADAPack x70 still cannot get a response after the retries, it will determine that it cannot communicate with the device, (see Configure Modbus Slave Device Configuration Settings).

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

The timeout value that you enter is for each scan.

Further Information

Link SCADAPack x70 Analog, Digital, or Counter Configuration items to the relevant Modbus Point Scanner: see Configure the Properties on the Mapping Tab.


Disclaimer

Geo SCADA Expert 2019