SCADAPack x70

Configure the Properties on the Mapping Tab

The Forms of SCADAPack x70 Analog, Digital, and Counter Configuration items include a Mapping tab. By default, the settings on this tab are disabled (the Mapping property is set to 'No Mapping').

You only need to set the 'Mapping' property to another option if one of the following applies:

Either:

and:

Or:


Disclaimer

Geo SCADA Expert 2019