SCADAPack x70

Configure the Out Of Range Limits

The SCADAPack x70 tab on the Forms of SCADAPack x70 Analog Configuration items contains an Out of Range Limits section. Use the section to specify the required limit values and define whether the SCADAPack x70 device generates an event whenever the analog exceeds any of those limits. The ability to generate events only applies when using a communications protocol that supports, and is configured to enable, event generation.

The limits specified in this section are independent of the minimum and maximum engineering values specified in the separate Scaling section of the tab.


Disclaimer

Geo SCADA Expert 2019