SCADAPack x70

Create Another Analog Configuration Item

Add another SCADAPack x70 Analog Configuration item to the database. This item will contain the configuration that you can download to the SCADAPack 575 for the analog output point that you will create for this tutorial.

When you create the item, you can leave most of the configuration fields at their default values.

On the SCADAPack x70 tab of the configuration Form, the only fields that you need to change for this tutorial are:

On the DNP3 tab, the only fields you need to change are:

Once you have configured this second Analog Configuration item, you can proceed to Create an Analog Output Point.

Further Information

For further information about configuring a SCADAPack x70 Analog Configuration item, see Set up Analog Configuration.


Disclaimer

Geo SCADA Expert 2019