SCADAPack x70

Minimum Configuration – Pulse Actions

This topic relates to Pulse Actions on the SCADAPack x70 driver.

When you add an item to the database, various properties on the item's configuration Form are assigned a value automatically. These default values are assigned on creation of the database item, to help reduce the amount of manual configuration that is required. As such, you only need configure a subset of the properties that exist on an item's configuration Form. Typically, the properties you have to configure include:

 

For a Pulse Action on this driver to be capable of functioning in Geo SCADA Expert, as a minimum you have to specify these properties on the Pulse Action's configuration Form:

 

Also ensure that the database items on which the Pulse Action depends are In Service, and have saved, valid configuration. This will produce a Pulse Action that is capable of functioning using the default configuration settings.


Disclaimer

Geo SCADA Expert 2019