Conditions

Syntax of conditions that can appear in a WHERE or HAVING clause.

Contents

Name Description
bool-condition Returns True if any of the bool-terms are True
bool-factor A single boolean factor preceeded with an optional NOT
bool-primary-between Returns True if a value is between two given values
bool-primary-comparison Returns the result of a comparison operation
bool-primary-exists Returns True if the result set is not empty
bool-primary-in Determines whether a given value matches any value in a query or a list
bool-primary-isnull Determines whether or not a given expression is NULL
bool-primary-like Returns True if a value matches a given pattern
bool-primary-like-regex Returns True if a value matches a regular expression
bool-primary-unique Returns True if all rows in the result set are unique (distinct)
bool-term Returns True if all of the bool-factors are True

Disclaimer

Geo SCADA Expert 2019