Alarm Banner Scripts

The Geo SCADA Expert Global scripting feature allows you to create scripts that provide additional functionality, for example, via the Alarm Banner in ViewX. Using VBScript, you can access the Alarm Banner Functions and Properties to:

To write the code for an Alarm Banner script, you will need an in-depth understanding of the VBScript language and an appreciation of the Alarm Banner functions and properties. You can write the code in the Global Script Editor.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

We also provide some examples of how Alarm Banner scripts can be used, Common Uses for Alarm Banner Scripts.


Disclaimer

Geo SCADA Expert 2019