Define which Explorer Bars a User can Access in ViewX and Virtual ViewX

The properties described in this topic apply both to User Forms and User Pattern Forms. (User Patterns only apply to systems on which Geo SCADA Expert can create new User accounts automatically as part of an External Authentication process. For more information, see Create User Accounts from a User Pattern.)

You can configure a user account so that users that log on via the account can only access certain Explorer Bars. For example, you can choose to limit a user account so that it only has access to the Queries Bar and cannot access the Database Bar or OPC Bars. This is useful when there are users that only require limited access to the system, for example, there may be management level users that only require access to the current data on the system and so only need to use the Queries Bar.

Use the ViewX tab on a User Form (or, if applicable, the User Pattern Form) to define which Explorer Bars a user can access when they log on from a ViewX or Virtual ViewX client:

  1. Either:

  2. Select the ViewX tab.
  3. Select the check box for each Explorer Bar that you want to be made available to the user that logs on via this account.

    The Explorer Bars are:

    Clear the check box for each explorer bar that you want to be unavailable to the user that logs on via this account.

  4. Save the configuration.

Disclaimer

Geo SCADA Expert 2019