Channel Settings

You can use the Channels section of the Geo SCADA Expert Server Configuration Tool to:

  1. Define the Settings for Channel Scanning Statistics Trends.
  2. Define how a PSTN Channel is Selected for Communications.
  3. Define the Settings for Modems .
  4. Define the Settings for COM Ports and TCP/IP Connections
  5. Define whether a Listen Port can be Shared.

The default settings are appropriate for many systems.


Disclaimer

Geo SCADA Expert 2019