Configure the Main and Backup Connections

Multi-server systems can use single or dual ethernet (dual network) connections between the servers.

When a single ethernet connection is used, there is only one connection and this is referred to as the ‘Main’ connection.

When dual ethernet connections are used, there are two connections—the ‘Main’ connection and a ‘Backup’ connection. The ‘Backup’ connection is only used if the ‘Main’ connection fails. If a failed ‘Main’ connection is restored, the server will stop using the ‘Backup’ connection and will return to using the ‘Main’ connection instead.

Dual ethernet connections can only be used with servers that support dual networking and have two network cards. Geo SCADA Expert only supports dual networking when:

If your server has 2 network cards that have the same subnet but do not support ‘teaming’, you can either:

or:

You can configure the settings for the ‘Main’ and ‘Backup’ connections on the Server Configuration Tool’s Partners tab:

To configure the Main Connection and Backup Connection settings, perform the following tasks on each server in the server architecture:

  1. Display the Server Configuration Tool and access the System Configuration>Partners settings.
  2. Define the Names/IP Addresses of the Other Servers.
  3. Define the Port Settings for a Server’s Connections.
  4. Define the Server Compression Settings.
  5. Define the ICMP Monitor Settings for a Server.

Disclaimer

Geo SCADA Expert 2019